This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UCD3138064A: when 35 & 36pin work in I2C mode, many of the bit fields are not used. Can you explain what fields are not used ?

Part Number: UCD3138064A


Tool/software: Code Composer Studio

when 35 & 36pin work in  I2C mode, many of the bit fields are not used.  Can you explain what fields  are not used ?

Can it affect other functions?

thanks

  • Basically, the I2C module is a PMBus module with 3 things removed:

    1.  slave mode support

    2. Alert line

    3. Control line

    Also, the PMBus hardware in master mode automatically inserts the byte with number of bytes in it into block messages.  This is not compatible with I2C, so it is removed from the I2C module.  So the bits removed are fairly obvious, but here is the list:

    PMBST or I2CST bits removed
      Bit 19: CONTROL_RAW
      Bit 18: ALERT_RAW
      Bit 17: CONTROL_EDGE
      Bit 16: ALERT_EDGE
      Bit 11: RPT_START
    PMBINTM or I2CINTM - bits removed
      Bit 7: CONTROL
      Bit 6: ALERT
    PMBCTRL2, PMBHSA – all removed, only deals with slave mode
    PMBCTRL3 or I2CCTRL3 – bits removed
      Bit 21: SLAVE_EN
      Bit 11: CNTL_DIR
      Bit 10: CNTL_VALUE
      Bit 9: CNTL_MODE
      Bit 8: ALERT_DIR
      Bit 7: ALERT_VALUE
      Bit 6: ALERT_MODE
      Bit 5: CNTL_INT_EDGE
    PMBCTRL3 or I2CCTRL3 – notes
      Bit 23: I2C_MODE_EN – present, but I2C is always enabled regardless of setting
      Bit 22: MASTER_EN – present, needs to be set for master to work

    This only affects the I2C interface, not anything else. 

  • thanks for your help .