This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24296: Can BQ24296 act as USB Host

Part Number: BQ24296

Hi,

Does BQ24296 detect a pen drive when connected to the same charging port through USB OTG cable.

  • Hey Sai Siri,

    No, the bq24296 cannot act as a USB communication class device. You would need extra circuitry/logic around the IC to perform the D+/D- communication and switching.

    What is the application here? Do you want the USB OTG to provide power AND communicate with the pen drive?


    Regards,
    Joel H