Hello PMIC Forum,
I am seeking a 5 Volt regulator for an energy conversion project.
My project converts mechanical energy in to electrical energy used to power consumer electronics. After the conversion, the output voltage from the converter is between 2 to 4 Volts. I need to regulate this converted voltage to 5 Volts that can source 200 mA to 500 mA. I am wondering if there is a TI product that can achieve this. I am looking for a regulator demo board that would help in my application.
Best regards,
Frank Hayden