This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110EVM-796: Do we have to have all 6 data log files for the GPC tool even if we do not need the SOC to be 100% accurate?

Part Number: BQ34110EVM-796
Other Parts Discussed in Thread: BQ34110

Hi we are currently using BQ34110 evm to measure the SOC of 12V 3.5Ah Lead-acid battery. 

1. Can we use the terminal voltage of the battery as 12.2V?

2. I see that we should use 1 configuration file and 6 data log files. Since we just want to see if the fuel gauging IC roughly reads the SOC of the battery, can we just test it with room temperature, 800mA discharge rate? Also, we are kind of in a hurry so we do not have time to execute all 6 discharging tests. If we can do it with just one test, do we upload 6 same files along with the configuration file? Or do we have to mock the values of temperature and make 6 distinct files?

Thank you very much in advance!