Part Number: TPS53355
Other Parts Discussed in Thread: TPS53667, TPS53647, LM3754, TPS40090-Q1, TPS40091, TPS40090, TPS546C23, PTH08T250W, PTV08T250W, PTV08040W, PTH12040W
My customer is currently using power with the TPS53355. The current output of the TPS53355 is 1V, 25A (input 12V).
We are looking for a larger load design than the current model. The desired current value is Continuous 50A.
Is there an IC that can be designed for this? Or can I implement it using two TPS53355s?
WEBENCH designed circuit with corresponding value. In this regard, the circuit is too complicated to use.