This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65911: TPS659113 NRND

Part Number: TPS65911

hi,

one of my customer is using TPS659113  . & now it is showing NRND . 

can i get to know the difference between TPS659113  &  TPS6591133  .

Regards

Mandar 

Arrow Electronics .

  • Hello Mandar,

    The only difference is that GPIO0 and GPIO7 have been swapped.  If the customer is switching from TPS659113, it may require a schematic change.  The following connections should be made per the TPS6591133 User's Guide to meet the latest processor sequencing requirements:

    If using TPS659113, GPIO0 should enable the 3.3V supply, and GPIO7 should enable the DDR supply.
    If using TPS6591133, GPIO0 should enable the DDR supply, and GPIO7 should enable the 3.3V supply.

    Regards,
    Karl