Part Number: BQ25505EVM-218
I have a BQ25505EVM-218 board and have made sure that it works by connecting a button cell (4 Volts) on VBAT_SEC/J8 and an LED with a 1k series resistor on VOR/J15; the LED lights, as you would expect.
I then disconnected the button cell and connected my intended energy source, a small wind turbine, to VIN_DC/J2, with the turbine not rotating. I reconnected the button cell on VBAT_SEC/J8 but now I cannot get my LED on VOR/J15 to light under any circumstances, even disconnecting everything and recreating the conditions of my first paragraph. VBAT_SEC/J8 still shows 4 Volts, VB_SEC_ON is still low but VSTOR and VOR/J15 never have any Volts on them.
Could I have damaged the BQ25505 part? The coils of my wind turbine measure 56 Ohms: could a low impedance on VIN_DC have caused damage? I can't see anything in the datasheet about this except a mention that if VIN_DC is higher than VSTOR and VSTOR is higher than VBAT_OV (which has never been the case here) then VIN_DC should be higher than 20 Ohms.