I'm finding these devices are failing. There is no fault indication with 3.6VDC on the input and 0.9VDC on the output. Power cycling the supplies does not clear the problem.
The load is a digital electronic circuit, is not inductive, and is attached through a 20" long 18AWG cable.
Peak current on the load is 1A pulsed for 30ms ON -> 1S OFF
The V3P3 is always on while the DUT_SRC (3.6VDC) is switched on and off at the upstream DUT Power Supply.
The DIO device resets at power up to all inputs. Subsequently the PG and FLT ports remain as inputs while the CE is set and an output. and those ports that are used remain as inputs. If there is an error where the DIO device drives the outputs of the TPS2421-1, would it cause a device failure of this nature?
If the bottom solder pad has a cold solder joint, could it cause this issue?