This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62130: Using 1uH inductor

Part Number: TLV62130

According to datasheet, we can use 1uH inductor with TLV62130.
In this case, datasheet says that FSW should be set Low.

When I design WEBENCH with the following use condition, Fsw becomes 1.2MHz although FSW is Low. And WEBENCH recommends 2.2uH.
However our customer want to use 1uH.
Can we use 1uH inductor with this using condition?

Vin: 12V
Vout: 1V
Iout: 2A
Ta: 85degC

Best Regards,
Kohei Sasaki