This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: TPS61099

Part Number: TPS61099

Dear Sir,

We have a question about TPS61099YFFR (or TPS61099YFFT) and found some of the boost converters have higher output voltage.

R1 and R2 set to 909k and 226k ohm with 1% tolerance.

To calculate the output voltage, I suppose we operate in PWM mode, the maximum output voltage should be

1.02 * (909*1.01) / (226*0.99) + 1.02 = 5.205V, but we measure around 5.22~5.24V for some unit.

After checking R1 and R2 at our side, we find they’re in the spec. of 1% tolerance but the output reference voltage is around 1.05V which is higher than we expect.

One thing can explain my measurement result is that we’re perform in PFM mode. If this is true, could you help answer following two questions?

  1. Does we provide all PFM mode TPS61099? Or this is a quasi-mode which decide by the load?
  2. What’s the upper and lower bound of reference voltage under PFM mode?

Thanks, Ian.