This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55332-Q1: Device selection in boost circuit

Part Number: TPS55332-Q1
Other Parts Discussed in Thread: TPS55340

Hi,

I am selecting the devices that can be used with the following specifications.
Application is a wireless power supply unit for residential equipment.
Due to the low input voltage, it is difficult to select the device.
However, I think that we can use the TPS55332-Q1 device, but can this device satisfy the specification?
(Since it is industrial, it does not have to be Q1 grade.)
Also, please let me know if you have other good devices.
If VIN = 2 V can not be accommodated, the specification can be changed to VIN = 3 V.

(Required specifications)
VIN: 2V to 12V
VOUT: 24V
IOUT: Peak 650mA (10ms), Average 100mA

Best regards,