Other Parts Discussed in Thread: , BQ25120A
Hi,
I have the BQ51013BRHL tied to the BQ25121 to charge the battery of the device I'm working on.
I found that there is an issue that when the board is slowly removed from the qi charging platform it will caused an increased Iq in the BQ25121 to up 1mA.
Then if I put it back on the qi charger and remove quickly the issue is resolved.
Seems like the low voltage or low slew rate of a qi charger loosing power causes the BQ25121 to glitch.
Is there a workaround to prevent this?