This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25940-Q1: Cout value of TPS25940-Q1

Part Number: TPS25940-Q1

Hi

Are there the calculation methods or recommending values of TPS25940-Q1's Cout?
My customer would like to use 22uF or 10uF as Cout.


Best regards,
Yokota
  • Hi Yokota

    There is no requirement for output capacitor. In datasheet, output capacitance is used to emulate capacitive load.
    Recommendation is 0.001 μF to 0.1 μF at input side only, to absorb the energy and dampen the transients at input of the device

    Best Regards,
    Rakesh