This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25120A: How to set ILIM, ISET, IPRETERM of BQ25120A?

Part Number: BQ25120A


I am developing a wearable product using BQ25120A.

Question 1)
I would like to connect ISET, ILIM, IPRETERM 3 pins directly to GND without using resistors. Can I set the values in the Register via I2C?

Question 2)

Can I open three ISET, ILIM, and PRETERM pins?
And can not I set the register value through I2C?

Question 3)
I do not use NTC, so I want to open the TS pin. Can I open the TS pin?

Thanks,

Sunbae Yim.