Other Parts Discussed in Thread: TLC555
hello,
I use TPS4H160B-Q1, 40V, 160mOhm, Quad Channel smart high side switch & TPS27S100B, 40V, 80mOhm, single channel high side switch for Over Current and Short circuit protection, but i found that this chip cant get proper result that i want.
Requirement:
1). Input Voltage - 24V/10A
2). Output Voltage - 24V/1A each Channel
3). Over Current protection
5). When short Circuit occurs in the device for any kind of the situation, than i want to Switch off the power for switch off my device, but whenever short circuit is removed automatically, than at a time that device is capable of provide me 24V/1A power a an output automatically not manually.
We use our device at long height like tower, so in case of water/weather in rainy time over device is in short circuit for short time. that's why our team not capable of solving that kind of problem each and every time at long height.
So, provide me complete circuit diagram and proper solution for that problem.
thanks,
Sudesh Verma
switch03@megastar.in
+91-7408398524