Other Parts Discussed in Thread: BQSTUDIO,
Hi,
I have a desing where the charger output is 6.15 V, so the battery does not charge.
This is the schematic of the charger. It can be powered by a 12V input or a 2s battery.
When I connect the 12V input, the output of the charger is 6.15V. When I connect the battery without the DC input, the output of the charger is the battery voltage.
If I connect both, the ouput is above 6.15V.
I can't connect by I2C port, and CH_OK pin is HIGH.
Where is the problem?