Hello,
I’m currently working in a circuit that uses a PN LMR23630ADDA from TI.
The aim is to have a DC/DC converter with input voltage from 9 to 36Vdc and the output voltage of 3.5Vdc.
I’m facing a behavior that I don’t know if it is a normal behavior.
When I switch the board on, after waiting for at least 2 minutes, the converter initializes without any problem. If I switch the board off and switch it on in less than 90 seconds after, the output voltage stays in 1.7Vdc approximately.
The only way to the converter starts without this behavior is if I wait more than 90 seconds before switching the board on.
Just to inform, there are two capacitors of 3300uF and one capacitor of 1500uF in the output of the converter. I’m aware that if I remove these large capacitors this behavior will be minimized, but I’m afraid of doing this once these capacitors came from an old circuit where they were necessary because of the Modem characteristics. During some events the Modem may need almost 2Amps.
Have you ever face this kind of situation with this converter? Is there any kind of workaround so that we can use the circuit in the way it is today?
I did not find a way to attach the schematic, please let me know if you need more information.
Thanks in advance,