Hi
My customer use BQ27542 and meet Flag SOC1 issue.
Status:
- Use HDQ通訊
- BTP SOC1 Set Threshold is “65535”
- in discharge process will continue comuniction to by HDQ
The issue is
- Start to discharge in SOC 15% (RSOC is about500mAh) ,the Flag SOC1 is 0
- Discharge battert till to the BQ27542 enable protection
- re charge battery to SOC15% but Flag SOC1 is 1 not reset to 0
so how to reset Flaag SOC1 to 0?
BRs
Eric LoJP_20180301.gg.rar