Hi,
Does BQ77905 support reverse charger protection? if not how to protect battery pack if the reversed charger is connect?
Alen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does BQ77905 support reverse charger protection? if not how to protect battery pack if the reversed charger is connect?
Alen
Hi WM,
Got it. thanks.
Two more questions,
Why does the circuit need a zener to clamp Vgs of CHGFET? I think a diode(1N4148) is enough, didn't see any risk that VGS exceed V(FETON) even if the voltage on Packe- goes to negative(Once the Vgs > Vth, the pack- will be back to 0V). How about your opinion? Are there is any thing I missed?
Do we need to add a zener to protect LD pin(or the ESD cell is strong enough) if a reversed charger is plugged in? I think the voltage on LD would exceed the ABS rating(20V) in this condition.
BTW, do you have any waveform about reverse charger protection? Will the SCD be triggered first when a reverse charger is plug-in?
Alen