This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24005: Wrong status indication

Part Number: BQ24005

Hi all,

We are using BQ24005 to charge a 7.4V battery.

We occasionally observe charging done indication (STAT1=High, STAT2=Low) even when the battery is not fully charged.

The indication resumes back to charging (STAT1=Low, STAT2=High) when we reset the power to the device.

It would be helpful if anyone can suggest the possible reason / solution for the specified issue.

Regards,

Felicita Mercy D.