Hi,
We are having problems performing a successful learning cycle using this device. We are using a 110Ah Lithium-Ion cell and our learning cycle procedure is as follows. The procedure has been put together using information from the datasheet (SLUSBX5B), the learning cycle procedure in document SLUA334B and advice from the 'Achieving a successful learning cycle' document (SLUA597).
- Start with a fully charged pack
- Set flash parameters, set chemID, perform calibration export .gg file
- Discharge at C/5 rate (22A) until termination voltage is reached
- Let the pack relax overnight (approx 16 hours)
- Send IT ENABLE command
- charge with CC/CV profile at C/5 rate (22A)
- Let the pack relax overnight (approx 16 hours)
- Discharge at C/5 rate (22A)
- Let the pack relax overnight (approx 16 hours)
- repeat 6 to 9 one more time
From the documentation, when we send IT_ENABLE the VOK and QEN flags should be set which is observed in our system. However after the first charge, update status is supposed to change to 5 and max error changes to 3% from 100%, neither of which are observed. For this reason we never get past step 7.
I have attached a a log file from the initial discharge and the first charge along with the .gg file and the .srec file of the configuration parameters.
Is there something wrong with this learning cycle? or have we set some parameters incorrectly?
I look forward to your response,
James