If the input voltage (7V nominal) and the regulated output voltage (9V @ 2A load), does the sync rectifier turned ON (fully?) or is it passed through it's body diode should the input voltage go higher than the output voltage to 12V?
What is the high side FET's body diode's current rating?