Hello E2E,
Is it possible for the max junction temp to equal max ambient operating temp on the LM76002-Q1, 125C?
Russell
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E,
Is it possible for the max junction temp to equal max ambient operating temp on the LM76002-Q1, 125C?
Russell
I am not sure what the context of you question is, however, the junction temperature will always be greater
than or equal to the ambient temperature. When the device is operating it will be dissipating a certain
amount of power. This will raise the junction temperature above ambient.
The specifications are stated for a cerain maximum junction temperature and the ambient
temperature that corresponds to this will depend on the power dissipation and thermal performance of the
board and device.