Dear Sir
I have use TPS56428 at 12V to 5V for USB port.
can I put 470uf cap at output side?
or any recommend for Max output cap value?
allen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
I have use TPS56428 at 12V to 5V for USB port.
can I put 470uf cap at output side?
or any recommend for Max output cap value?
allen
Hi
The value of Cout in the datasheet is the 20uF~68uF, so you had better do not use the 470uF. Bigger cap means smaller cross frequency which will cause unstable.
Besides, is the 470uF Electrolytic capacitor? The TPS56428 is DCAP2 -mode, the ceramic capacitor or low ESR cap is better.
Hi Quote
Yes, 470uF is Electrolytic capacitor.
Our design need supply 5V to USB port, and USB port need input cap bigger than 120uF, if we put 120uF ceramic capacitor at TPS56428 output side is that OK?
Allen
yes, 120uF is ok, but the transient performance will be not very good. Thank you!