This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI teams,
When we use LM22676 or LM22674, we design the circuit as below, the FB signal is from the MCP6002. The output voltage is changed following the DAC output signal.
But when we PP the product, and do test, LM22676 burn up when the system is power up. The failure rate is about 10%, and when finish power up , the system is steady. Can you help to check whether the circuit is OK ? and pls. give some advise. thanks
It looks like you have the feedback from the output going through another device.
The FB input is very sensitive and may be causing some kind of trouble. I would test
your boards with the FB input connected through the FB divider directly and see if that helps.
Also, be sure that the inductor and diode are both rated for the full current limit of the regulator.
You can return the damged units to TI for evaluation if you wish.