This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22965: Effect of Input Capacitance on Vout Rise Time (tR)

Part Number: TPS22965

I would like to use a 4.7 uF as the input capacitance. Will equation 1 in the datasheet be affected by the input capacitance value? I ask because the table that follows equation 1 specifies typical rise time values with the note that CIN = 1 uF.