This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: Icout calculation for slua479b application note

Guru 19645 points
Part Number: UCC28070

Question about slua479b application note(attached below), Page-5 equation (15).

Icout_hf become minus current on the condition of Pout: 3300W, Vin_min: 180V, Vout:390V.

(Icout_lf is 6.83A by equation (14))

When above case, which UCC28070 operation ① or ②? 

①Actually, Icout_hf flow 0A current.

②Icout_hf should not become minus current, this is no recommended condition.

 ⇒If correct is ②, please let me know operation principle.

Best regards,

Satoshi