Other Parts Discussed in Thread: TPS3306
What is the input impedance of Switch Control Pin(C2) on TPS22924C (LOAD SWITCH) IC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Venkatesh,
Can you please help us understand why this information is needed? The ON pin does not have any pull down circuitry to bring the pin voltage down. It is a high impedance pin, and the leakage current spec can be found in the datasheet.
Thanks,
Alek Kaknevicius
Hi Venky,
The input impedance of the ON pin will be very high, in the range of megaohms. Another way to look at this is checking the max leakage current for the pin. At 3.6V, the max leakage current is specified as 0.1uA. By using R = V/I, the minimum impedance of the pin can be estimated as 36MΩ.
Is this impedance acceptable?
Thanks,
Alek Kaknevicius