My Customer is using the UCC28515 in an AC-DC power supply. It is intended for use at 60Hz, but it accidentally got designed into a 400Hz application, and while it runs OK if fails conducted EMC testing.
In the application information of the data sheet there is some equations for calculating values for the loops, and there is a reference schematic on page 23 – which I assume is for 60Hz.
Is there is a reference design for the UCC28515 with an AC input at 400Hz? or a spreadsheet calculator to assist with design?
It does NOT have to still run at 50/60Hz. (If it can, great – but it doesn’t have to)
Specs of the power supply are in the attached Excel File.