I'm using the BQ25895 to power an ARM SOC. The USB signals are routed to both the BQ25895 and the USB port of the ARM SOC.
When I connect the BQ25895 to a charger, how do I prevent the ARM SOC from interfering with the "Input Source Type Detection" process? I would like the BQ25895 to draw the maximum current available from the charger.
Thank you.