This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: Zero input offset: how does it affect CM pin output

Part Number: LM5117


Dear All,

I'd like to understand how to interpret this specification when it comes to calculating voltage on CM pin at a given load current.

What I have interpreted is that if offset is 25mV, then with 4 mOhm current sense resistor, I may read no voltage on CM pin until minimum load current is 357mA. (25mV / 4mOhm * 17.5). Is this understanding correct?

Also, is this offset bidirectional?

Regards,

Sourabh