Hi, I want to use bq24617 in my project, my requiment is as follows
1. Vin (Adapter) 5 to 14 V and I need VSYS (System power) = 4.5V
2. battery: 1S cell li-ION battery charging.
3. battery charging current= 5A and adapter input current = 8A.
in reference schematics the system power is drived from input but i want the power after buck conversion so that my system power will be always near to 4.5V. is it possible to modify the circuit like this. do you have any reference circuit similar like my requirement if so please share with me.