This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM25088: WEBENCH part disappeared

Part Number: LM25088

Tool/software: WEBENCH® Design Tools

I used WEBENCH on 08 March 2018 for a non-isolated dc-dc converter with the following specs:

  • VinMin = 21.6V
  • VinMax = 26.4V
  • Vout = 19V
  • Iout = 6.316A
  • Temp = 60 degC

The solution I chose at that time was the LM25088 because we use it on a similar design.

Now, (15 March 2018) I try those parameters or any other parameters, and the LM25088 does not show up as a solution at all.

I looked at the webpage for the LM25088 and it is not listed as "obsolete" or "not recommended for new designs"

Why would the solution disappear?

Has anyone experienced similar issues with other parts?