I am looking for a precision 5 VDC regulator. It is powered by about 8 VDC. A current of 1 amp is sufficient. I need a TO-220 3 pin package. This is to be a direct replacement for a 2940 regulator. Pinouts are pin 1 for input, pin 2 for GND, and pin 3 for Output. I need an industrial temperature range. The output voltage is 5.00 +/- .05 VDC max. Any suggestions?