Part Number: TPS92310-12FB
Dear Sir:
Does TPS92310-12FB EVM can support AC TRIAC dimming control?
Best Regard
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS92310-12FB
Dear Sir:
Does TPS92310-12FB EVM can support AC TRIAC dimming control?
Best Regard
Jason
Hello Jason,
Our expert is out until Monday, but there may be. I will forward this to him and look into it. I hope to have an answer for you soon.
Regards,
Clint
Dear Sir:
We want to used TPS92310 to design indoor lighting and we want it can support AC90~130 input and DC20~45V output (32mA , 13W), BTW , Can I modify TPS92310-12FB to meet PM6013 for Triac dimmable AC-DC LED driver?
Best Regard
Jason
Hello Jason,
Yes, it can be modified to triac dim however you may not be able to get 13W from that design, transformer and certain component limits. I assume you mean 320 mA not 32 mA? 45V * 320 mA = 14.4W.
You will have to add the input resistor that needs to be able to handle continuous pulses since it will be charging the EMI and damper capacitors when the triac fires. This is R2 on PMP6013. The value and power dissipation will depend on the EMI capacitor values, damper capacitor value and output power.
You will also need the damper circuit, R1 and C1 to keep the triac from mis-firing. (the values will depend on your power level and EMI capacitor values
Then you will have to add the Compensation circuitry, R22, R24, C13, Q2 and R17. This may need tuning to the dimming performance you desire.
This is an open loop dimming circuit so changes in line voltage will show up in the light output.
Regards,
Dear Sir:
Due to our U.S customer have requirement of PE>85% & PF>95% for AC to DC triac dimming control and our competitor is LTC LT3799 , It can meet both conditions as PE>85% & PF>95%(at AC120V,Vout=33~34V,vout current=320mA) , If we want to replace LT3799 , customer hope we can confirm TPS92310 can meet same specification , Does TPS92310 can meet this specification? or TI have another solution can do that? BTW , If used different Traic , does it will have different influences?(LUTRON-PD-6WCL / LUTRON-DVEL-300P / LUTRON-CT-603PG).
Best Regard
Jason
Hello,
If you plan on using this with 21-39 volt output as one design and triac dimming you will probably need to add a voltage regulator to the primary bias winding because the range gets too large for VCC. The Wurth transformer 750341087 isn't too far off from a turns ratio standpoint though it is probably too small for your higher power. This will be a custom transformer, Wurth can make it to your design requirements, or some other manufacturer you can work with.
If the secondary winding and primary bias are the same turns ratio then VCC would run from about 21 to 39 volts, lower when you triac dim. 39 is too high and why you would want to put a voltage regulator on the primary bias winding (a resistor, zener and transistor or MOSFET). If you picked 1:0.8 then 21 volt output would leave 16.8V on the primary bias and when triac dimming it would not have enough voltage to stay on. I picked 5:1 for the primary to secondary winding, it can vary depending on which power components you wish to use.
The tool is limited in what you can do with it, I set it close to what you are looking for:
I would go through the datasheet equations for all operating points to make sure it works as desired.
Regards,