Hello
Datasheet of TPS78227 shows that we need to connect both ground pins together.
Part is pin to pin compatible with an On semi Ldo except on one ground pin taht is left open on the On Semi part.
PCB is already done with On Semi part, but we would like to use the Ti part instead.
Question 1 :
Can we leabve one of the ground pin open ?
Question 2 :
If not, can we tie together the ground pin with a 0.1ohm resistor made with a strap in 0603 format (datasheet of the 0 ohm strap specify a max resistance of 0.1ohm).
What would be the influence of the 0.1ohm resistor if any on the stability ?
Thank you very much.
With best regards, Alain