Other Parts Discussed in Thread: LM20144
Hi at all people.
I have a strange problem with LM20144 device. I attached here the project and simulation that i realized on Texas WEBDESIGN .
I have realized a board where I have 5 DCDC with LM20144, different voltages. The problem is ONLY with LM20144 1Vout 2A.
All circuits have the same layout , same circuit, different inductance and FB resistors, obviously, BUT all other DCDC run correctly at 1.8Vout, 3.3Vout, 2.5Vout, 1,2Vout. For all DCDC the same Vin: 5V
Just only 1,0Vout doesn't run correctly: in output I measure 1,2V, Vfb = 0,91V (error) and PGood, obvious, LOW level.
I don't understand if this is a LM problem.
Inside the datasheet i can see that is characterized until 1.2Vout.... that is the limit ?
Thanks at all for help that You would to do to me in this little problem.
Regards
PS: I don't find attach possibility .... how can I send You my simulation file ?