Part Number: TPS40170
Hi Sir,
May I double confirm with you, Our customer used the TPS40170, if AOC=4.5, then we can open the RLDRV(R5) right?
Iocp(min)=8A
Iripple=2.4A
MOSFET is CSD87350
RDS(on)Q1=5mohm
RDS(on)Q2=1.1mohm
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.