Hello,
I use TPS 2490 as a soft start (inrush limiter) in dv/dt mode on a high power motor driver board. The bulk capacitance on the load side is 25000uF and the working voltage is 30V. I would like to identify if there exist any (theoretical) condition on the inputs/outputs of the 2490 chip that will cause the soft start to re-activate while the load (motor) is running because that will destroy the FET! For example, what will happen if there are glitches on Vcc or Enable while the motor is running? On the load side there is, except for the motor, a motor controller and MCU. The motor is started several seconds after initial power up and then runs continuously. Downstream dc/dc is not synchronized by PG. Enable pin is controlled by an MCU powered from the primary side. Please help me identify possible scenarios that will re-activate the soft start which will burn the FET and ways of avoiding this to happen.
Thank you for your help.