Hello Team,
The recommended value of Cin in the data sheet is stated as follows.
・Cin = 10~22uF (300mAmax)
Is it necessary to use the same Cin even when Iout=100mA(max)?
Currently, 4.7uF x 2 is used. Is there a problem?
Best regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
The recommended value of Cin in the data sheet is stated as follows.
・Cin = 10~22uF (300mAmax)
Is it necessary to use the same Cin even when Iout=100mA(max)?
Currently, 4.7uF x 2 is used. Is there a problem?
Best regards,
Kato
Hi Kato,
if the datasheet does not mention, that the input capacitance may be decreased if the output current is only 100mA, then I would not decrease the input capacitance. This input cap is used for the stability of the regulator. Allthough the output of a regulator looks stable, there's a fast acting control circuit in every regulator, which has to be stabilized by caps at the input and output. It's wise to follow the datasheet recommendations quite precisely. Esepecially if it is a LDO!
What kind of input cap do you use? Is it a X7R or X5R? Take care, these caps can show a drastical decrease of capacitance when applying higher DC voltages. Do you have a datasheet of this cap?
Kai