Hi Team,
We develop a smps using ucc28251. And my question is the pulse from the device(ucc28251) is not varying linearly. when it starts to regulate the output voltage,pulse width keeps on changing like D=0.45 to 0.1 but the output voltage is constant. Because of that the transformer making humming sound. Why so? If input voltage is higher than that of required output voltage, then the duty cycle should be low right? but in this case the pulse width is oscillating from high to low. Reply to me as soon as possible thanks.