This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92515HVEVM-749: TPS92515HVEVM-749 J1 replacment

Part Number: TPS92515HVEVM-749

Dear TI,

I have TPS92515HVEVM-749 High Current buck LED Driver Evaluation Module. I see that ILED can be set with Jumper J1. For my purpose I need to replace Jumper with Switch/Analog MUX or Micro Solid State Relay with control signal. Can your recommend such ASIC?

and I also want to ask what happen if I force 5V on IADJ pin?

In my application I need for 1400 ms 36 mA ILED, then 90 ms break ( no ILED), then 190 ms 1000 mA ILED and again 90ms break. All this will be in loop.

Thanks a lot for any suggestions

BR

Marcin