We need 23VDC @ 5A output, 24VDC to 60VDC input, 72VDC input withstanding; small footprint. Really want 24VDC output, but 23VDC was the best any of the TI calculators could handle. Any comments on selection of the LM5145 for this application? Some background: we started with a TPS40170RGYT design, but we had some input voltage noise spikes over 60VDC and we had several boards where the circuit failed and the IC actually had a hole blown out of the top of the package. Also, WEBENCH asks for multiple input and output capacitors because of the low ESR. Is it okay to substitute a high capacitance electrolytic and a few low-ESR ceramics?