I would like to estimate the amount of current the TPS73701 LDO will "add" depending on the ourput current running through it.
I believe the common term for this is "Quiescent Current".
Unfortunately, I couldn't find any reference to this term in the data sheet.
My questions are as follows:
1. Is the meaning of the symbol I_GND (GND pin current) in the data sheet, equivalent to the "Quiescent Current"?
2. The data sheet states that when I_OUT=10mA, typically we'll get I_GND=400uA. What is the typical I_GND for I_OUT in the range of 0.5mA-1mA?
3. The above mentioned values appears in the data sheet under the assumptions that V_IN=V_OUT+1 and V_EN=2.2V. Will I_GND be significantly impacted if V_IN and V_EN are significantly higher?
Thanks in advance!
Tal Ben-Porath