This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62160: questions around remote sensing for this device

Part Number: TPS62160


One of my customers is looking for some confirmation on the following:

Regarding implementing the approach laid out in "Remote Sensing for Power Supplies"  (slyt467), to account for IR losses in the power-distribution-network from the SMPS to the SoC load, can we confirm if this approach is supported with the TPS62160QDSGTQ1?

If yes:

  • TPS62160QDSGTQ1 has both a FB and VOS pin. Which would go to the load?
  • VOS is listed as voltage sense and connection for control loop circuitry
  • Looking for confirmation if one or both of these would be tapped off at the load

Note- the remote sensor is located at approximately 1.5 - 2 inches from the load.