This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: OCVTAKEN not clearing during relax

Part Number: BQ34Z100-G1

Hi,

I'm using a scaled deep cycle Pba Battery with a chem id of 808.

I'm not getting successful learning cycles.

One issue I see is that I may not be entering a relax mode after discharge because the OCVTAKEN flag bit does not clear and get reset.

I suspect it has to do with my taper current, quit current, and charge and discharge current settings but I don't see anything wrong with the settings in accordance with documentation.

Can you examine my log file and gg file and help me?

Thank you in advance.

-Tim

CHM0 bat6 CHMID808 X (03-14-2018).zip