Other Parts Discussed in Thread: BQ24650
Dear Sir, I attach my schematic. When I plug in the battery(5-series Li battery, the voltage is about 21V), the bq24610(U100), Low side MOS(Q103, connect to LODRV) and Zener Diode(D101, connect to REGN) will be burned out. At this time, the external DC adapter is not pluged in(I do not add the DC_IN_24V). In other words, I just plug in the battery then the bq24610(U100), Low side MOS(Q103) and Zener Diode(D101) are burned out. If the bq24610(U100), Low side MOS(Q103) and Zener Diode(D101) are not burned out luckly, the charging process can be proceed successfully. The Q103 and bq24610 are grounded to Analog GND. Could you help provide the solution? thanks.