Other Parts Discussed in Thread: BQ76940, BQ78350
Hi,
We have an issue with shutdown that seems to be related to temperature. We have an MCU that uses the SMBus to read data values from the BMS and also controls when to shut down. The procedure we use to shut down is:
- MCU sends MAC Shutdown
- MCU reads the operation status register until the SDM bit is set, then it seizes all communication (so as not to wake the BMS again)
- BMS is supposed to shut down, hence disable the 2.5V LDO from the AFE (bq76940)
However, when we do our climatic tests the BMS does not shut down after setting the SDM bit, instead i clears the bit and continues to operate. When this occurs, the UTD protection has been activated (we have the threshold set to -20°C).
This procedure work well when in room temperature, even with simulated temperature sensors at -20°C and UTD present.
I cannot find any reference to why the BMS does not shut down, also I read in sluubd3c section 17.2.10:
"Once SHUTDOWN mode is enabled, it is not possible to clear it without entering SHUTDOWN mode".
Which does not seem to be correct, the SHUTDOWN mode is never entered (what I can detect atleast).
Can you please shed some light on this?
Best regards
Emanuel W