Hi there,
I've noticed some inaccurate current measuring values with my implementation of the BQ76930. I've tested different currents from 1A to 20A ( or even 25-30A) with a Fluke Current clamp and a constant current load. The Shunt-resistor is 2mOhms. ( SCD should be 120A, OCD around 80-100A) Usually the device will need 15-20 A with 40A only for 1 sec max.
Here are some values i've measured, does anyone know what could be the reason for that problem?
Kind regards,
Alex
| UNI-T UT139B Multimeter | Power supply | BQ76930 with 10mOhm Shunt |
| 1,919 | 1,98 | 2,021 |
| 2,055 | 2,11 | 2,165 |
| 2,494 | 2,55 | 2,631 |
| 3,011 | 3,07 | 3,185 |
| 3,955 | 4,01 | 4,199 |
| 3,491 | 3,55 | 3,714 |
| 4,004 | 4,06 | 4,269 |
| 4,49 | 4,56 | 4,189 |
| 5,02 | 5,08 | 5,392 |
| 5,49 | 5,56 | 5,935 |
| 5,98 | 6,05 | 6,516 |
| 6,51 | 6,57 | 7,091 |
| 6,98 | 7,05 | 7,634 |
| Agilent Multimeter | Power supply | BQ76930 with 10mOhm Shunt |
| 0,24 | 0,29 | 0,252 |
| 0,531 | 0,58 | 0,555 |
| 1,037 | 1,09 | 1,085 |
| 1,239 | 1,29 | 1,297 |
| 1,532 | 1,59 | 1,606 |
| 1,733 | 1,79 | 1,819 |
| 2,024 | 2,08 | 2,125 |
| 2,566 | 2,62 | 2,698 |
| Fluke Current Clamp | BQ76930 with 2mOhm Shunt |
| 1,08 | 1,11 |
| 2,09 | 2,165 |
| 3,05 | 3,161 |
| 4,01 | 4,178 |
| 5,02 | 5,25 |
| 6,06 | 6,247 |
| 7,08 | 7,431 |
| 8,1 | 8,529 |
| 9,07 | 9,579 |
| 10,29 | 10,909 |
| 11,19 | 11,841 |
| 12,04 | 12,85 |
| 13,11 | 14,069 |
| 14,13 | 15,365 |
| 15,08 | 16,081 |
| 16,09 | 16,963 |
| 17,1 | 17,754 |
| 18,13 | 19,015 |
| 19,08 | 19,864 |
| 20,15 | 21,151 |
| 21,24 | 21,298 |
| 24,98 | 26,936 |
| 30,07 | 31,566 |