This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24618: Setting Adapter Current Regulation for a 10A charger

Part Number: BQ24618

Hi, I'm using this part to make a 10A charger. In the datasheet it says "up to 10A Charge current and Adapter Current". Should I set the resistors for ACSET and ISET1 to limit the Adapter input and Charge Current to 10A? Or can/ should I set the resistors for the ACSET to the actual limit of the AC adapter (10.7A) and set the charge current to 10A?

 Thanks,

JP